{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What can cause the ATV630 and ATV930 drives to have a blank display and not power up?

Article available in these languages: Spanish

Issue:
ATV630 and ATV930 drives with blank display and not power up.

Product Line:
Altivar ATV630 and ATV930

Environment:
All

Cause:
DC bus is not charging, bad power board or MCB

Resolution:
  1. Check Mains voltage on L1 L2 L3,
  2. Check DC bus voltage on PA+ and PC if it has the voltage on the ATV930 drives only
  3. Check the +24vdc and +10vdc power supplies.
  4. Power cycled  if needed  and see if the display comes back up.
  5. Check to see if there is an  Ethernet cable connected into the modbus port.

Schneider Electric Nigeria