{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How can I reload the custom parameter set stored inside the drive memory from last saved on the ATV212 or S-Flex?
Issue:
How can I reload the parameters stored  in the drive from the factory or from last saved configuration on the ATV212 or S-Flex?

Product Line:
ATV212 including the S-Flex enclosed drives.

Environment:
All

Cause:
Change in programming or application requires the drive to be reset to factory default settings and reload last saved custom parameter inside the drive memory

Resolution:
If a program had been saved to the drive as using tyP set to 7, then the saved file can be restored by changing tyP to 8.

d

Consult the ATV212 Programming manual for additional information: https://www.se.com/us/en/download/document/S1A53838/

Schneider Electric Nigeria

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: