{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
PM5500 devices are not logging onboard data in Power Monitoring Expert 8.2

Issue
PM5500's not downloading onboard logs

Product Line
Power Monitoring Expert 8.2

PM5500 series meters

Environment
Web Application

ION Reporter

Cause
DataLog Recorder states were being rolled back upon network router restarts and communications loss.

Resolution
A new driver was released for the device type in Power Monitoring Expert 8.2. Contact Technical Support for updated device driver download.

Schneider Electric Nigeria