{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can you configure ION Meters to accept multiple 61850 clients?
There are absolutely no settings that you can change in your ION Meter regarding number of accepted Client connections.

That is hardcoded in the meter's firmware, no matter which communication protocol is used to connect to the meter.


Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.