{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How can the ATV12 Drive run a motor up to 400Hz?
Issue:
ATV12 drive capability to run a motor up to 400Hz

Product Line:
Altivar 12, ATV12

Environment:
All

Cause:
Wants to run the motor up to 400hz

Resolution:

Programming the drive

DRC menu
bFr=60hz
UNS = motor voltage
Ncr motor current
FRS= 400hz
tFr =400hz

Main menu
ACC=3 seconds suggested 10 seconds
DEC 3 seconds
LSP 0 (for a test, set 400hz if you do not have a voltage or current feedback speed input)
HSP 400hz

Schneider Electric Nigeria