{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Why are CVS upstream and downstream customer connections (terminal) different in thickness?

This is what the design is. The thickness of upstream and downstream connection is not the same, while the connection location is the same as shown in the picture below, for CVS400/630, the dimension C1=C2=26, which make sure the firm connection of the same cable or bar on upstream and downstream connection.

Schneider Electric Nigeria

Attachment(s)

rtaImage.jpgrtaImage.jpg [26.27 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: