{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
PME 8.1 Diagnostic File Error

Issue:
After running the Diagnostic Tool, a .CAB file is never created.

Product:
Power Monitoring Expert

Environment:
Power Monitoring Software

Resolution:
There are 2 possible solutions below.
  1. A workaround would be unchecking the check box "Compress Package" in the tool so that you will get the diagnostic folder contains all the info.
2. PME installer CD, there is 'DiagnosticsTool_x86.exe' under the folder \setup\Installers. You can use this to reinstall the tool.

If you do not have the installation CD, you may download the installation files for the latest PME versions below.  Please check what version you are running before using the installation file.


Power Monitoring Expert 9.0

Power Monitoring Expert 8.2

Power Monitoring Expert 7.2





Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.