{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Do ATV320 Drives have Real Time Clock built-in?
Issue:
Real Time Clock built-in on the ATV320.

Product Line:
ATV320

Environment:
All

Cause:
Need time stamp on Faults

Resolution:
No, ATV320 drives do not have Real Time Clock in them. Therefore, there is no Time Stamp in the Fault History.

Schneider Electric Nigeria