{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is SCADAPack Configurator (Standard) for SCADAPack Workbench?

Issue

Why do I need SCADAPack Configurator for SCADAPack Standard? Previously I was only using ISaGRAF 3.55 to program my SCADAPack.

Product Line

SCADAPack Standard RTU Line

Environment

ISaGRAF 3.55, SCADAPack Workbench

Resolution

Previously in ISaGRAF 3.55, the end user would need to write the SCADAPack controller settings (serial port, DNP3, RTC, etc...) by using the Write to Controller command via the Tools > Controller drop down menu. Specific SCADAPack Standard functionality (advanced telemetry functions) is not built into the new Workbench as it was in 3.55. Instead a separate software package called SCADAPack Configurator is needed to perform these operations. Along with being able to read and write all the specific SCADAPack Standard specific settings, SCADAPack Configurator can be used to obtain Watchdog logs, logs obtained from the dlogfcfg & dlogf functions, DNP Master and Slave diagnostics, C/C++ program Loader as well as SCADAPack Security.

SCADAPack Configurator Logo

Where to Download
https://shop.exchange.se.com/en-US/apps/62860/scadapack-workbench-and-utilities

Schneider Electric Nigeria

Explore more
Range:
SCADAPack 300, 32SCADAPack 50
Explore more
Range:
SCADAPack 300, 32SCADAPack 50
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.