{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What do the different colors mean on the LED indicator for the Thermal Monitoring solution installed in the Model 6 Motor Control Center

An external single LED status indicator is provided on the unit disconnect mechanism for displaying thermal status conditions.

Solid Green - OK No Alarms                                        No Color / Black - Not Operating / Loss of Power to Device
Solid Yellow - Phase Temperature Imbalance        Flashing Yellow - Line / Load Delta Thermal
Flashing Red - High Temperature                                Solid Red - Sensor Failure Signal Loss


Temperature Alarms are configurable by dip switches.

The Thermal Monitoring solution includes Modbus RS485 serial communications capability. iMCC Network solutions with this feature are available under special order configurations.

For detailed installation and setup information reference the Exertherm instruction bulletin

For pricing and lead time information contact the Technical Assistance Group at the Seneca, SC manufacturing location.

Schneider Electric Nigeria