Unity Pro offers the Write _Input_Int block which can be used to accomplish either task. The video linked to this FAQ will demonstrate this functionality using an M340. The information is also valid for M580 and Quantum PLC's.
Released for:Schneider Electric Nigeria
Explore more
Range:
Modicon Quantum
Modicon M340
Modicon M580
Articles that might be helpful
Show more articles
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.