{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can you power up the ATV32 with an external 24Vdc supply?
Issue:
ATV32 power up with an external 24Vdc supply

Product Line:
ATV32

Environment:
All serial numbers

Cause:
To maintain control power to the drive.

Resolution:
Yes, the P24 terminal and COM are the connections that can be used for external 24VDC.
**NOTE:  This does not apply to the ATV320, the P24 terminal on ATV320 is only used to supply the STO (Safe Torque Off) terminal, P24 will not accept 24v.

Schneider Electric Nigeria