{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
PowerChute Business Edition unsuccessfully installing on Linux after multiple installations on the server

Issue:

After multiple installations of PowerChute Business Edition on the same Linux server, a rpmdb PANIC can occur, resulting in the following error message, “rpmdb: PANIC: fatal region error detected; run recovery”. This error message is due to the rpm database becoming corrupted, and requiring a rebuild.

Product:
PowerChute Business Edition v9.5

Environment:

Linux operating systems

Solution:

Follow the steps below to rebuild the rpm database and successfully install PowerChute:

  1. If a yum repository has been configured on the Linux server, clean the cache using the following command:
yum clean-all
  1. Remove the rpm database packages and rebuild the database:
rm -f/var/lib/rpm/_db*
rpm --rebuilddb
  1. Install PowerChute Business Edition using the rpm install commands:
  1. For v9.5
rpm -ivh pbeagent-9.5.0-301.XX.rpm

NOTE: The above command will differ for 32-bit and 64-but Linux operating systems.
32-bit Linux: rpm pbeagent-9.5.0-301.i386.rpm
64-bit Linux: rpm pbeagent-9.5.0-301.x86_64.rpm
  1. For v10
rpm -ivh pbeagent-10.0.0-301-XX.x86_64.rpm
NOTE: The above command will differ based on your locale.
English:  rpm -ivh pbeagent-10.0.0-301-EN.x86_64.rpm
Chinese: rpm -ivh pbeagent-10.0.0-301-CN.x86_64.rpm
  1. PowerChute Business Edition successfully installs without rpm database errors.
NOTE: This issue has been resolved in PowerChute Business Edition v10.0 which is available to download on the APC website.

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.