{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Why would a shorting contactor have a lower amperage rating than the motor being used?
Issue:
Shorting contactor with lower amperage rating than the motor.

Product Line:
Altistart Soft Starters with shorting contactors

Resolution:
Shorting contactors are usually derated by one size unless you have the full voltage bypass option. This is because the shorting contactor pulls in after the motor is up to full speed from being ramped up by the Soft Starter. So the full amperage rating is not needed since the contactor is not ramping the motor up from zero. However, if you're using a full voltage bypass, the shorting contactor needs to be matched up with the motor amperage.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Nigeria