Search FAQs
LXM28 fault AL5A1 and Wn720
Issue: LXM28 fault AL5A1 Product Line: LXM28 Lexium 28 all part numbers Resolution: AL5A1 and Wn720 are two faults that remain after the production process. This is a known issue that was already fixed and new drives are now manufactured without this fault. The way of removing these two faults is by resetting the drive to factory settings via P2-08=10. No need to re-flash the firmware |
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: