Search FAQs
Does the Bacnet card for ATV600 drive support star or ring topology?
Issue:
When the ATV600 is used on a Bacnet network, is a star or ring topology supported?
Product line:
ATV630, VW3A3725
Environment:
All models, All serial numbers.
Cause:
Bacnet Communications
Resolution:
No. Bacnet should be connected in a daisy chain configuration only.
When the ATV600 is used on a Bacnet network, is a star or ring topology supported?
Product line:
ATV630, VW3A3725
Environment:
All models, All serial numbers.
Cause:
Bacnet Communications
Resolution:
No. Bacnet should be connected in a daisy chain configuration only.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: