{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Sepam 2000 D22 and D32 applications - are remote measurements available to be accessed using Modbus for these applications?
For the majority of the legacy Sepam 2000 application types, it is possible to read measurements such as current and voltage remotely using Modbus communication.

However, for the D22 and D32 application types, attempting to read from the Modbus registers that are used for other application types (e.g., T04, S02) will result in zeros being returned.

Based on the latest information available at the time of writing of this document, Remote Measurements are not available for the Sepam 2000 D22 and D32 application types.

AEDL3

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.