{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the maximum disturbance recording time?

Maximum recording time depends on configuration; number of channels set to be recorded and sampling rate for the recordings. If the recording time for one record is shorter than maximum time the device will have more buffers. Maximum number of buffers is 12.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
move-arrow-top