{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Why does the ATV630 drive trip on EPF2 Fault after installing the BACnet Card?
Issue:
ATV630 getting an EPF2 Fault after installing the BACnet Card.

Product Line:
ATV600, ATV630, ATV660

Environment:
All

Cause:
NA

Resolution:
Check the Profile Setting. If it is set for I/O profile then change it to Separate or Not Separate. However, changing I/O profile puts you back to factory settings. Therefore, all the VFD settings have to be programmed again.

Schneider Electric Nigeria