{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the process to cycle input power to a variable frequency drive in order to reboot it?
Issue:
Drive has detected a fault that requires a reboot of the drive to clear

Product Line:
All Altivar products.

Environment:
All

Cause:
Reboot needed to clear latched fault code.

Resolution:
To properly reboot an Altivar VFD, disconnect three phase input power from the L1, L2, L3 terminals. Observe the main display of the drive, it will remain lit for some time after power is removed to the drive, between a few seconds to a few minutes depending on the horsepower of the drive. Once the main display shuts off, wait another 5-10 seconds before reapplying power to the drive. Failure to allow sufficient time before reapplying power to the drive can cause the fault code to remain latched in the drive.

Schneider Electric Nigeria