Search FAQs
What is the size of the cutting in partition wall for passing through a Canalis KS element?
For easy handling and installation a 50mm distance to the wall on each side of the KS element should be considered.
Two rules have to be followed for correct installation:
- No junction block at level of partition, for maintenance purpose;
- If at the level of partition the cutting in the wall will be filled with plaster, it must not be on a tap-off outlet.
Two rules have to be followed for correct installation:
- No junction block at level of partition, for maintenance purpose;
- If at the level of partition the cutting in the wall will be filled with plaster, it must not be on a tap-off outlet.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: