{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the minimum distance between the Vigirex rectangular sensor and the following bending of the busbar?
Depending on the size of the sensor, the following minimum distances must be respected:
- 280 x 115 mm sensor -> the distance between the sensor and the busbar bending must be equal to, or higher than 25cm.
- 470 x 160 mm sensor -> the distance between the sensor and the busbar bending must be equal to, or higher than 30cm.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: