{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the EMKA 1150-U56, -U56-01, -U58 be installed into a NetShelter SX cabinet?
Issue:
We are unsure if the EMKA electromechanical release door handle will fit onto a NetShleter SX cabinet.

Product Line:
NetShelter SX

Environment:
All models, all serial numbers.

Cause:
A customer wants to install the EMKA electromechanical release door handle onto a NetShelter SX cabinet.

Resolution:
Yes, the EMKA 1150-U56, 1150-U56-01 and 1150-U58 can be installed onto a NetShelter SX cabinet, but you must reuse the NetShleter SX cam.

Schneider Electric Nigeria