Issue:
ATV630 Process Drives Bacnet option cards availability.
Product Line:
Altivar ATV630 only
Resolution:
The BACnet part number is VW3A3725, is a BACnet MS/TP module for ATV600 series drives. They are not compatible with ATV900 series drives.
Note that the ATV630, ATV650, ATV680, and ATV660 drive Firmware needs to be minimum V1.8.
ATV630 Process Drives Bacnet option cards availability.
Product Line:
Altivar ATV630 only
Resolution:
The BACnet part number is VW3A3725, is a BACnet MS/TP module for ATV600 series drives. They are not compatible with ATV900 series drives.
Note that the ATV630, ATV650, ATV680, and ATV660 drive Firmware needs to be minimum V1.8.
Released for:Schneider Electric Nigeria