Search FAQs
Why can't I see entries like FR1, CHCF, or CD1 in CoE in ATV320 VFDs with VW3A3601 EtherCAT comm card?
Issue:
Entries like FR1, CHCF, or CD1 in CoE in ATV320 VFDs with VW3A3601 EtherCAT comm card.
Product Line:
ATV320
Environment:
All
Cause:
Having access to these parameters through CoE allows easier configuration and also the potential for automated configuration.
Resolution:
Need V1.12 ESI file. It corrects the problem.
Entries like FR1, CHCF, or CD1 in CoE in ATV320 VFDs with VW3A3601 EtherCAT comm card.
Product Line:
ATV320
Environment:
All
Cause:
Having access to these parameters through CoE allows easier configuration and also the potential for automated configuration.
Resolution:
Need V1.12 ESI file. It corrects the problem.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: