{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What would cause a EPF2 fault using Profinet's telegram 1 and I/O profile on the ATV630 and ATV930 drives?

Issue:
EPF2 fault causes using Profinet and I/O profile on the ATV630 and ATV930 drives.

Product Line:
ATV630, ATV930

Environment:
All

Cause:
IO Profile and Telegram 1 are not compatible.

Resolution:
Profinet telegram 1 is not supported with IO Profile.  It is suggested that they use telegram 100 which does support IO Profile.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: