Search FAQs
What is the maximum allowed temperature rise on the terminal connections of the Compact INS switch disconnectors?
The INS devices are tested and certified according to standard IEC 60947-3. Temperature rise tests are performed at the rated operational current Ie.
The maximal allowed temperature can be calculated as ambient temperature (temperature of air around the device) + maximum temperature rise limit.
The standard specifies temperature rise limit on the terminals for external connectors at 80K.
For example - if ambient air temperature is 40 deg. C, then maximum allowed temperature on terminals for external connection is: 40 + 80 = 120 deg. C
The maximal allowed temperature can be calculated as ambient temperature (temperature of air around the device) + maximum temperature rise limit.
The standard specifies temperature rise limit on the terminals for external connectors at 80K.
For example - if ambient air temperature is 40 deg. C, then maximum allowed temperature on terminals for external connection is: 40 + 80 = 120 deg. C
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: