{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is there a parameter in the ATV212 that will change the output phase rotation/direction of the motor?
Issue:
ATV212 phase rotation swap parameter

Product Line:
ATV212/ATV21

Environment:
All

Cause:
Output phase rotation

Resolution:
No. To change the output phase rotation on the ATV21 / ATV212, you must swap 2 of the motor leads.

Schneider Electric Nigeria