{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the specs for the fiber optic communication in the ION 8650 meter
Issue
Want to know the specification of fiber optic communication with the ION8650 meter

Product Line
ION8650

Environment
Fiber optic communication

Resolution
The part used for fiber optic communication is AFBR-5803AQZ from Broadcom Link to site.
Connector TypeSC
Data Rate125 MBd
EmitterLED
Fiber TypeMultimode Glass
Maximum Distance (m)2000
Nominal Optical Wavelength (nm)1300

Schneider Electric Nigeria