What energy parameters are measured by PM1130H meter ?
The meter provides uni-directional, 2-quadrant, Class 1 / Class 0.5 accurate energy metering. The meter stores accumulated value of any one of the selected energy from active, reactive, or apparent energy in nonvolatile memory: • Delivered (Utility): kWh, kVARh, kVAh • Delivered (Alternate Source): kWh, kVARh, kVAh • Total (Utility + Alternate Source): kWh, kVARh, kVAh Under the condition when Source 1 = Utility and Source 2 = Genset or DG.
Released for:Schneider Electric Nigeria
Explore more
Range:
EasyLogic PM2000 series
Articles that might be helpful
Show more articles
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.