{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What can cause the Vijeo Designer simulation build not to run?
Issue:
Vijeo Designer simulation does not start

Product Line:
Vijeo Designer

Resolution:
This is only one of many possible reasons why the simulation does not run. If you install Vijeo Designer 6.2 SPx while Windows Defender was running, it can cause the simulation build not to run.

Turn off the Windows Defender and re-install Vijeo Designer 6.2 SPx.

Schneider Electric Nigeria