Search FAQs
Looking for handle kit for B frame Powerpact breaker for through-the-door breaker operation?
Issue:
Throug the door handle kit for B Frame powerpact breaker.Product Line:
PowerPact B breakers
Environment:
PowerPact B-Frame Moulded Case Circuit Breakers
Cause:
It is often necessary operate breakers from outside of the enclosure they are installed in when they are not used in a Schneider panelboard
Resolution:
You can use the following;
LV426932 or LV426933
Released for:Schneider Electric Nigeria
Explore more
Category:
Range:
Explore more
Category:
Range: