{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is there an Assembly number that can be tied to the user map in the Tesys T LTMR product?

Issue:
Customer needs to tie the user map registers to an assembly number in order to reduce traffic on his network from explicit messaging.

Product Line:
LTMR Tesys T product.

Environment:
All models, All serial numbers.

Cause:
Unable to find supporting documentation.

Resolution:
There is no pre-defined instance in the Tesys-T that points to the user table.  Customer will need to either access this via explicit messaging or use instance 116 to pull all monitoring registers and then discard those that are not needed.

Schneider Electric Nigeria