{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What can cause an LSTP fault on ATV21 or ATV212 Drives?

Issue:
LStP alarm code on ATV21/212.

Product Line:
ATV21, ATV212, S-Flex

Environment:
All

Cause:
NA

Resolution:
LSTP is not a fault, but rather an alarm for Low Speed Stop. It is an Auto-stop based on continuous operation of the VFD at speeds below a threshold (LL + F391) for a period of time (F256).
Check to see if the automatic stop function with F256 was activated.  To deactivate, set F256 = 0.
The VFD will continue to run in LStP alarm until it gets a speed reference above the threshold (LL+F391).
To deactivate the LStP alarm, increase the Command Frequency to a value above the Low Speed threshold (LL+F391) or turn off the Run Command.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: