{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Whether ATV212 is compatible with Pasive Harmonic Filter

We cannot connect the passive filter due to C less capacitor which enter in resonance with the DC bus. There is no offer with ATV212 to reach 5% THDI.
Basically the drive is designed to reach 48% THDI, but no input filter offer is existing to decrease the THDI (neither line choke nor active filter).
The target of this product is to compliant with the standart IEC61000-3-12 so THDi above 48%. Our product achieve around 35% of THDi.

Schneider Electric Nigeria

Explore more
Range:
Altivar 212
Explore more
Range:
Altivar 212
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.