{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the ATV600 or ATV900 be programmed to always run at one constant speed?
Issue:
Programming ATV930 to run at constant speed.

Product Line:
Altivar Process ATV600 and ATV900 series

Resolution:
To run, any drive needs both a run command (to start running) and a speed reference (how fast to run).
To run at one constant speed, the speed reference needs to stay constant.  In the absence of any speed reference, the drive will default to the Low Speed setting.

In the Simply Start menu, set Low speed to the desired constant speed.  To prevent anything from giving a higher reference you could also set High speed = Low speed.  Alternatively, you can assign both the Forward run and a Preset Speed to the same input to always have the drive run at the same speed.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Nigeria