{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Which version of Vijeo Designer supports the HMIDT752 and HMIDT952?

Issue:

What version of Vijeo Designer supports the HMIDT752 and HMIDT952 screens for the  Harmony (formerly known as Magelis) HMIGTU series?

Product Line:

Vijeo Designer, Harmony (formerly known as Magelis) HMIGTU

Resolution:

The HMIG5U2 is the current HMI CPU/Motherboard rear module in Vijeo Designer v6.2 that supports the HMIDT752 (15" Wide) and HMIDT952 (19" Wide) Touchscreens (as of August 2019).

Vijeo Designer v6.2 Service Pack 9 provides the HMIG3U the ability to use these touchscreens.

See the Table below for HMIGTU series support for these screens for each Vijeo Designer v6.2 Service Pack:

ModelService Pack 6 or olderService Pack 7Service Pack 8Service Pack 9
HMIG2UN/AN/AXX
HMIG3UXXXO
HMIG5UXXXX
HMIG5U2XOOO


Legend:
N/A - HMIG2U not introduced yet in this Service Pack

X - does not support the HMIDT752 or HMIDT952
O - supports the HMIDT752 or HMIDT952

Note:
In EcoStruxure Operator Terminal HMI configuration software (versions: Vijeo XD v3.0 or EcoStruxure Operator Terminal Expert v3.1+), both the HMIG3U and HMIG5U2 can use the HMIDT752 and HMIDT952 displays.
This is a different configuration software than Vijeo Designer.

Schneider Electric Nigeria