{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How can it be verified the motor is running through the shorting contactor and not the ATS48?
Issue:
Validate motor is running through the shorting contactor, not the soft starter.

Product Line:
ATS48

Environment:
All serial numbers

Cause:
Testing the contactor

Resolution:
Verify the r2A and r2C is closed.
Measure motor current on the load side of the shorting contactor.

Schneider Electric Nigeria