{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the Unity Pro version compatible with the PRM Gateway DTM v1.3.0.0?
Issue
This resolution clarifies the minimum version of Unity Pro compatible with the PRM Gateway DTM v1.3.0.0.

Product Line
EcoStruxure Control Expert, M580, PRM (TCSEGPA23F14F)

Environment
Unity Pro v11.1, BMEP581020 v2.50, PRM

Resolution
The PRM gateway DTM v1.3.0.0 is compatible with Unity Pro v11.1 or later.

Schneider Electric Nigeria