Search FAQs
Frequently Asked Questions (FAQs) for UPS Network Management Card 2 (NMC2)
Issue:
This FAQ document answers commonly-asked questions about UPS Network Management Card 2 (NMC2) SmartSlot Cards, the firmware features and its benefits. It also addresses the questions of UPS Network Management Card 1 (AP9618) users to migrate to UPS Network Management Card 2 (AP9630, AP9631 and AP9635).
Product line:
All the Product Installed with Network management card - NMC 2
Environment:
All models, All serial numbers
Cause:
Frequently Asked Questions (FAQs) for UPS Network Management Card 2 (NMC2)
Resolution:
Please find attached the PDF document to clarify the below questions.
- What are the main benefits of the UPS NMC 2?
- What features are new to UPS NMC 2 firmware?
- How do the UPS NMC 2 SKUs differ between features?
- What are the security features in the latest UPS NMC 2 firmware?
- What are the accessories supported by UPS Network Management Card 2? (dry contacts, environment sensors, expansion chassis)
- What can UPS Network Management Card 2 be integrated with Building Management Systems (BMS)?
- Where can I try out the new UPS NMC 2?
- Is UPS NMC 2 compatible with all single phase SmartSlot UPSs
- Does UPS NMC 2 integrate with StruxureWare Data Center Expert and InfraStruxure Manager?
- Does UPS NMC 2 offer out of band management?
- Can UPS NMC 2 be used simultaneously with PowerChute Business Edition using serial/USB communication?
- How do UPS Network Management 2 features compare with that of UPS Network Management 1?
Released for:Schneider Electric Nigeria
Attachment(s)
Explore more
Range:
Explore more
Range: