Search FAQs
Which motor control type should be used for a pump or fan application on an ATV630 Drive?
Issue:
On an ATV630 what motor control type should be used for a pump or fan application?
Product Line:
Altivar 630
Environment:
Pump or fan applications
Cause:
Basic programming
Resolution:
U/F VC Quad should be used for pumps and fans.
In some applications that require higher starting torque other motor control types may be required.
Please see the ATV600 Programming Manual for additional details:
https://www.se.com/ww/en/download/document/EAV64318/
If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)
On an ATV630 what motor control type should be used for a pump or fan application?
Product Line:
Altivar 630
Environment:
Pump or fan applications
Cause:
Basic programming
Resolution:
U/F VC Quad should be used for pumps and fans.
In some applications that require higher starting torque other motor control types may be required.
Please see the ATV600 Programming Manual for additional details:
https://www.se.com/ww/en/download/document/EAV64318/
If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: