Search FAQs
Can you use a Servo stepper motor on the ATV600 and ATV900 Process drives?
Issue:
ATV600 and ATV900 process drive running a servo stepper motor.
Product Line:
ATV600 and ATV900 Process drives
Environment:
All
Cause:
Wants to run a stepper motor on the ATV960 drive.
Resolution:
No you can not run a stepper motor on the ATV600 and ATV900 process drives. You will need to look a the Servo Lexium drive.
ATV600 and ATV900 process drive running a servo stepper motor.
Product Line:
ATV600 and ATV900 Process drives
Environment:
All
Cause:
Wants to run a stepper motor on the ATV960 drive.
Resolution:
No you can not run a stepper motor on the ATV600 and ATV900 process drives. You will need to look a the Servo Lexium drive.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: