{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Unity Pro, how to create variables with a name having more than 32 characters.
Unity Pro allows name  of 32 charaters maximum for elementary variables
The solution to have more characters is to structure the variable using DDT.
By this way you will have nearly no more limitation  (it is possible to have nested DDT up to 15 levels).

Example:
Define the DDT variable

Intanciate the variable

use the variable: this variable has more than 32 characters

Schneider Electric Nigeria