{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the ATV630 and ATV930 Process Drive be used on a Resistance Grounded (IT), Corner Grounded or Ungrounded power System?
Issue:
Can the Process Drive be used on a different types of 3 phase power connectoins?

Product Line:
Process Drive

Environment:
All

Cause:
IT system
Ungrounded system
Corner grounded delta

Resolution:
Yes.  With any of these systems the internal EMC Filter must be disconnected according to the instructions in the Installation Manual.
Warning message

ATV600 Installation manual link: https://www.se.com/ww/en/download/document/EAV64301/
ATV900 Installation manual link: https://www.se.com/ww/en/download/document/NHA80932/

Schneider Electric Nigeria