Search FAQs
Video: How to configure a register through ION Setup 3.0
Issue
Configuring Modbus Registers on PowerLogic ION Meters via ION Setup
Product Line
PM8000
ION8650
ION8600
ION7650, ION7550
ION7600, ION7500, ION7400
Environment
ION Setup 3.0
Cause
Would like to map values that aren't already mapped in the Modbus register map
Resolution
Follow the steps to configure a register in ION Setup 3.0
Open ION Setup 3.0 > View Setup Screens > Open Setup Assistant
Navigate to Communications > 3rd Party Protocols > Modbus Slave tab
![](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000008zrLwQAI&oid=00DA0000000abSm)
Click on the Map name to highlight to Edit the map
![](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000008zrOgQAI&oid=00DA0000000abSm)
Click Add, then configure the parameters of the custom register.
Note: the Address value must be between 40001 & 41800
![](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000008zrOuQAI&oid=00DA0000000abSm)
Select a Source Register to link
![](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000008zrKuQAI&oid=00DA0000000abSm)
Click Ok after parameters are chosen
Can save the Modbus map as a CSV by clicking on 'Save As' and choosing a file location. Click Ok
Now a Modbus register has been added/configured and can read this register's value
Note: For documentation on ION Modules, please reference ION Reference
Configuring Modbus Registers on PowerLogic ION Meters via ION Setup
Product Line
PM8000
ION8650
ION8600
ION7650, ION7550
ION7600, ION7500, ION7400
Environment
ION Setup 3.0
Cause
Would like to map values that aren't already mapped in the Modbus register map
Resolution
Follow the steps to configure a register in ION Setup 3.0
Open ION Setup 3.0 > View Setup Screens > Open Setup Assistant
Navigate to Communications > 3rd Party Protocols > Modbus Slave tab
Click on the Map name to highlight to Edit the map
Click Add, then configure the parameters of the custom register.
Note: the Address value must be between 40001 & 41800
Select a Source Register to link
Click Ok after parameters are chosen
Can save the Modbus map as a CSV by clicking on 'Save As' and choosing a file location. Click Ok
Now a Modbus register has been added/configured and can read this register's value
Note: For documentation on ION Modules, please reference ION Reference
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: