{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Assigning an IP address in a Unity Momentum processor via bootp server does not work with firmware version 2.0.
Issue
A Unity Momentum processor with firmware V2.0 installed will not allow an IP address to be assigned via bootp/DHCP server.


Product Line
The processors affected are 171CBU90890 and 171CBU98091.


Resolution
The IP assignment via bootp server issue is fixed in Unity Momentum firmware version 2.01 and higher.
IP address assignment via bootp/DHCP server does function correctly with firmware versions 1.31 and lower.

Schneider Electric Nigeria