How many BMXNOR0200 module we can have with Modicon M340 CPU
The maximum Ethernet port for M340 CPU system is 3 including the port on PLC. Therefore, a maximum of two BMXNOR0200 modules can be inserted in a M340 system.
Released for:Schneider Electric Nigeria
Explore more
Range:
Modicon M340
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.