Search FAQs
What are the Vijeo Designer v6.2 Runtime specifications/limitations?
Issue:
What are the Vijeo Designer v6.2 Runtime specifications/limitations?
Product Line:
Vijeo Designer, XBTGC/GK/GT, HMIGK/GTO/GTU/STO/STU, iPC, Panel PC, Box PC
Resolution:
Below are the Runtime specifications for Vijeo Designer v6.2.
The user application you create in the Editor is restricted by target machine run-time specifications. The following table lists the memory capacity of available target machines. DRAM memory affects how much information you can display on the panel at one time. Internal Memory affects the total size of your application. SRAM memory affects how much information you can store between run-time sessions.
If you are using a tablet/smartphone, the memory capacity depends on the model. See the manufacturer's specifications for more information.
*1 The XBTGT5430 model comes in two versions that differ in their DRAM size (32 MB or 64 MB). To determine the version of the XBTGT5430, look for the following serial numbers on the manufacturer's label on your target machine:
What are the Vijeo Designer v6.2 Runtime specifications/limitations?
Product Line:
Vijeo Designer, XBTGC/GK/GT, HMIGK/GTO/GTU/STO/STU, iPC, Panel PC, Box PC
Resolution:
Below are the Runtime specifications for Vijeo Designer v6.2.
Run-Time Specifications
- Use the following statistics as only a guideline for creating your own applications. Some applications may not be able to run despite remaining below these documented numbers because of memory limitations. To make sure your application will run correctly, check the memory requirement for each panel and operation, and compare these requirements with your target machine. For details, see Section 25.3.3, Checking Memory Usage. Always test your application thoroughly before running it in a production environment.
- The following statistics were obtained by testing each individually on factory machines. These numbers will vary depending on the operating environment, the complexity of the application, the CPU load, and the amount of memory available on the target machine. Some of these performance numbers can be enhanced with upgraded memory, CF Cards/SD Cards, and hard disks.
Panels | |||||
Number of panels/popup windows (limit) | The number of panels that can be created in a project depends on the amount of flash memory available on your target machine and on the size of each panel. For example, you can have a project on an XBTGT6330 target that contains 100 panels. As the number of panels for your project increases, memory consumption also increases. | ||||
Number of objects on a panel (recommended) | The number of objects that can be placed on a panel depends on the target machine's panel height and width. For example, you can have a project on an XBTGT6330 target that contains 200 objects per panel. As the number of objects placed on a panel increases, memory consumption also increases. | ||||
Popup windows (limit) | Number of popup windows that can be displayed at run time: maximum of 3, which includes the popup keypad. | ||||
Large Toolchest parts | On some targets, large parts placed on a panel may cause a wait time to occur when changing panels. For example, on an XBTGC 2230U, switching from one panel to another panel with a Web Browser took several seconds. | ||||
Actions | |||||
Maximum number of actions | 100 | ||||
Scripts | |||||
Maximum length of each script (recommended) For other script recommendations, see Section 18.3.4, Key Points. | 50 lines | ||||
Error Logging | |||||
Number of run-time events stored | 100 | ||||
Alarms and Events | |||||
Number of Alarm Groups and Event Groups in a Target (limit) | 32 max. | ||||
Number of Alarm Categories and Remote Categories in a Target (limit) | 32 max. | ||||
Number of event records in an event group (limit) | The number of event records you can store in each event group is 10,000 max. Events are recorded in both History and Log, which results in having two event records for each event that occurs. For example, if you set 10,000 as the maximum number of total records, you can only store 5000 events. | ||||
Number of alarms in alarm groups (limit) | The number of Log and History alarm records you can store in each alarm group is 10,000 max. In the Alarms node, when Backup Alarm Group is set to No, you can store up to 80,000 total Log and History alarms in a target's alarm groups. When Backup Alarm Group is Yes, the number of alarms is limited by the space available on SRAM. | ||||
Number of alarms in an alarm category (limit) and remote category | 60,000 | ||||
Alarm Backup The size required by each alarm message depends on the alarm type. Active: 20 bytes per record History: 24 bytes per record Log: 16 bytes per record | SRAM Capacity (Backup) is different for each target machine type. 128 to 512 KB (Depends on model. Refer to your hardware manual.) For information about how much SRAM is required by your project, see Section 4.5.1, Target Properties. | ||||
Number of attachments per e-mail | 1 max. | ||||
Maximum size of file attachment | 10 MB | ||||
Link Objects | |||||
Maximum number of definition objects (per Target node) | 100 | ||||
Maximum of folder levels in the folder structure for definition objects (per Target node) | 5 | ||||
Files | |||||
Number of text files (limit) | 200 max. | ||||
Text file size (recommended) | 50KB max. | ||||
Number of video files (limit) | 200 max. | ||||
Number of sound files (limit) | HMIG5U / HMIG5U2 / iPC / XBTGTW Series | HMIG3U / XBTGC / XBTGT / XBTGH / HMIGTO / HMISTO / HMISTU / HMISCU / HMIGK Series | XBTGK Series | ||
1,500 | 200 | 200 | |||
Languages | |||||
Number of user languages you can create (allowed) | 15 max. | ||||
Variables | |||||
Number of variables per panel (limit) | HMIG5U / HMIG5U2 / iPC Series | All other target types | |||
Maximum 2500 variables per panel | Maximum 800 variables per panel. | ||||
Number of variables per target (limit) | HMIG5U / HMIG5U2 / iPC / XBTGTW Series | HMIG3U / XBTGC / XBTGT / XBTGH / HMIGTO / HMISTO / HMISTU / HMISCU / HMIGK Series | XBTGK Series | ||
12000 max. | 8000 max. | 8000 max. | |||
NOTE:
| |||||
Number of variables you can share (recommended) | HMIG5U / HMIG5U2 / iPC / XBTGTW Series | HMIG3U / XBTGC / XBTGT / XBTGH / HMIGTO / HMISTO / HMISTU / HMISCU / HMIGK Series | XBTGK Series | ||
400 | 300 | 300 | |||
NOTE:
| |||||
Security | |||||
Number of security groups per target | 20 max. | ||||
Number of users per security group | 100 max. | ||||
Number of users per target | 100 max. | ||||
Number of users per Vijeo Designer project | 200 max. | ||||
Driver Restrictions on Windows Target Machines | |||||
Biometric Switch | The Biometric Switch's USB driver currently does not support Windows target machines running on embedded Windows operating systems, including Windows XP Embedded and Windows Embedded 7. | ||||
Drivers not supported on target machines that run Windows operating systems | The following drivers are not supported on Windows operating systems, and therefore Windows target machines cannot connect to physical equipment using these drivers. Simulation in Buildtime is also not supported. Schneider Electric:
| ||||
Data Logging | |||||
Number of Data Logging Groups in a target (limit) | 80 | ||||
Maximum number of variables being logged in a target | HMIG5U / HMIG5U2 / iPC / XBTGTW Series | HMIG3U / XBTGT1005 / XBTGT2000 and higher / XBTGC / XBTGK / HMIGTO / HMISCU / HMIGK Series | HMISTO / HMISTU Series | XBTGH Series | |
250 variables max. | 100 variables max. | 60 variables max. | 80 variables max. | ||
Table Resources | |||||
Maximum number of table resources in a tablet/smartphone project | 10 | ||||
Maximum number of states in a table resource | 255 | ||||
Resource Library | |||||
Maximum number of Text, Color, Image, Font Resources in a project (limit) | 256 | ||||
Maximum size of an image file used in an image resource | 1920x1080 | ||||
Forms Printing | |||||
Number of forms you can create for each user application (limit) | 50 max. | ||||
Maximum number of objects on one form (recommended) | 2000 | ||||
Communication | |||||
Number of equipment nodes (limit) | HMIG5U / HMIG5U2 / iPC / XBTGTW Series | HMIG3U / XBTGC / XBTGT / XBTGH / HMIGTO / HMISTO / HMISTU / HMISCU / HMIGK Series | XBTGK Series | ||
80 max. | 48 max. | 48 max. | |||
Number of scan groups per equipment (limit) | 20 max. per equipment node | ||||
Number of Maximum Share Connections (limit) | HMIG5U / HMIG5U2 / iPC / XBTGTW Series | HMIG3U / XBTGC / XBTGT / XBTGH / HMIGTO / HMISTU / HMIGK / HMISCU Series | XBTGK Series | ||
32 | 8 | 8 | |||
NOTE:
| |||||
Recipe | |||||
Total number of recipe groups (standard recipe group or Parison Recipe Group) per target | 32 max. | ||||
Number of recipes in a recipe group (limit) | 256 max. | ||||
Number of ingredients in each recipe (limit) for a standard recipe group | 1024 max. | ||||
Number of ingredients in each recipe (limit) for a Parison Recipe Group | 64 min. 400 max. |
The user application you create in the Editor is restricted by target machine run-time specifications. The following table lists the memory capacity of available target machines. DRAM memory affects how much information you can display on the panel at one time. Internal Memory affects the total size of your application. SRAM memory affects how much information you can store between run-time sessions.
If you are using a tablet/smartphone, the memory capacity depends on the model. See the manufacturer's specifications for more information.
Target Machine | Memory (DRAM) | Storage Media / Internal Memory (Flash Memory) | Memory (SRAM) | |
Magelis iPC | Compact MPC KT52 | 256 or 512 MB | N.A. | 2 MB (Simulated) |
Compact MPC KT22 | 512 or 1024 MB | N.A. | 2 MB (Simulated) | |
Compact MPC KT12 | 512 or 1024 MB | N.A. | 512 KB | |
Compact MPC KT55xx2 | 512, 1024, or 2048 MB | N.A. | 512 KB | |
Compact MPC KT22xxx20 | 512 MB | N.A. | 512 KB | |
Compact PC Box MPC KN02 | 512 MB | N.A. | 512 KB | |
Smart MPC ST52 | 256, 512, or 1024 MB | N.A. | 2 MB (Simulated) | |
Smart MPC ST21 | 256, 512, or 1024 MB | N.A. | 2 MB (Simulated) | |
Smart MPC ST11 | 256 or 512 MB | N.A. | 512 KB | |
Smart/Smart+ MPC ST52xx2/HMI PSx7 | 256, 512, or 1024 MB | N.A. | 512 KB | |
Smart Box MPC SN01 | 256 MB | N.A. | 512 KB | |
Smart MPC ST21xxx20 | 512 MB | N.A. | 512 KB | |
Flex PC Box PTX MPC02 | 512 MB | N.A. | 2 MB (Simulated) | |
Flex PC Box PTX MPC05 | 512 MB | N.A. | 2 MB (Simulated) | |
Box Performance HMIBPxxx2 | 2-8 GB | Storage media | 512 KB | |
Box Performance HMIBPxxx5 | 2-8 GB | Storage media | 512 KB | |
Box Universal HMIBUxxx1 | 1-3 GB | Storage media | 512 KB | |
Box Universal HMIBUxxx2 | 1-3 GB | Storage media | 512 KB | |
HMIGTW5354/Panel W HMIPWC5 | 1-2 GB | Storage media | 512 KB | |
HMIGTW7354x/Panel Optimum HMI PWC7/PVC7 | 1-2 GB | Storage media | 512 KB | |
Panel Performance HMIPPx6 | 4 GB DDR3 (in 1 slot) | Storage media | 2 MB (Simulated) or Interface Option ports (IF and IF2) | |
Panel Performance HMI PPx7/PRx7 | 2-8 GB | Storage media | 512 KB | |
Panel Performance HMIPPx9 | 2-8 GB | Storage media | 512 KB | |
Panel Universal HMIPUx6 | 2 GB DDR3 (in 1 slot) | Storage media | 2 MB (Simulated) or Interface Option ports (IF and IF2) | |
Panel Universal HMI PUx7/PTx7 | 1-3 GB | Storage media | 512 KB | |
Panel Universal HMIPUx9 | 1-3 GB | Storage media | 512 KB | |
XBTGTW450 | 512 MB | N.A. | 2 MB (Simulated) | |
XBTGTW652 | 256, 512, or 1024 MB | N.A. | 2 MB (Simulated) | |
XBTGTW750/HMIGTW7353 | 512 MB | N.A. | 2 MB (Simulated) | |
Rack PC Optimized HMIRSO/HMIRXO | 2 GB | Storage media | Use Internal Flash to simulate SRAM. | |
Rack PC Universal HMIRSU | 4 GB | Storage media | Use Internal Flash to simulate SRAM. | |
Rack PC Performance HMIRSP | 4 GB | Storage media | Use Internal Flash to simulate SRAM. | |
S-BOX PC Optimized HMIBSO | 2 GB | Storage media | Use Internal Flash to simulate SRAM. | |
S-BOX PC Universal HMIBSU | 4 GB | Storage media | Use Internal Flash to simulate SRAM. | |
S-Panel Performance HMIPSPx7 | 8 GB | Storage media | 2 MB (Simulated) or Interface Option ports (IF and IF2) | |
S-Panel Performance HMIPSPx9 | 8 GB | Storage media | 2 MB (Simulated) or Interface Option ports (IF and IF2) | |
Enclosed PC Performance HMIPEPx9 | 8 GB | Storage media | 2 MB (Simulated) | |
S-Panel Optimized HMIPSOx5 | 4 GB | Storage media | 2 MB (Simulated) or Interface Option ports (IF and IF2) | |
S-Panel Optimized HMIPSOx7 | 4 GB | Storage media | 2 MB (Simulated) or Interface Option ports (IF and IF2) | |
Box Universal HMIBMU | 4 GB | Storage media | 512 KB | |
Performance HMIBMP | 8 GB | Storage media | 512 KB | |
Magelis HMIGTO Series | HMIGTO1300 | 128 MB | 64 MB | 128 KB |
HMIGTO1310 | 128 MB | 96 MB | 512 KB | |
HMIGTO2300 | 128 MB | 64 MB | 128 KB | |
HMIGTO2310 | 128 MB | 96 MB | 512 KB | |
HMIGTO2315 | 128 MB | 96 MB | 512 KB | |
HMIGTO3510 | 128 MB | 96 MB | 128 KB | |
HMIGTO4310 | 128 MB | 96 MB | 512 KB | |
HMIGTO5310 | 128 MB | 96 MB | 512 KB | |
HMIGTO5315 | 128 MB | 96 MB | 512 KB | |
HMIGTO6310 | 128 MB | 96 MB | 512 KB | |
HMIGTO6315 | 128 MB | 96 MB | 512 KB | |
Magelis HMIGTU Series | HMIG3U | 256 MB | 1 GB | 512 KB |
HMIG5U | 2 GB | 16 GB | 512 KB | |
HMIG5U2 | 2 GB | 16 GB | 512 KB | |
Magelis HMISCU Series | HMISAC (HMIS65/S85) | 128 MB | 128 MB | 128 KB |
HMISBC (HMIS65/S85) | 128 MB | 128 MB | 128 KB | |
Magelis HMISTO Series | HMISTO501 | 32 MB | 16 MB | 128 KB (Simulated) |
HMISTO511 | 32 MB | 16 MB | 128 KB (Simulated) | |
HMISTO512 | 32 MB | 16 MB | 128 KB (Simulated) | |
HMISTO531 | 32 MB | 16 MB | 128 KB (Simulated) | |
HMISTO532 | 32 MB | 16 MB | 128 KB (Simulated) | |
Magelis HMISTU Series | HMISTU655 | 32 MB | 16 MB | 64 KB |
HMISTU855 | 32 MB | 16 MB | 64 KB | |
HMIS5T | 64 MB | 32 MB | 64 KB | |
Magelis XBTGT Series | XBTGT7340 | 64 MB | 32 MB | 512 KB |
XBTGT6340 | 64 MB | 32 MB | 512 KB | |
XBTGT6330 | 32 MB | 32 MB | 512 KB | |
XBTGT5430 | 32 or 64 MB*1 | 32 MB | 512 KB | |
XBTGT5340 | 64 MB | 32 MB | 512 KB | |
XBTGT5330 | 32 MB | 32 MB | 512 KB | |
XBTGT5230 | 32 MB | 32 MB | 512 KB | |
XBTGT4340 | 64 MB | 32 MB | 512 KB | |
XBTGT4330 | 32 MB | 32 MB | 512 KB | |
XBTGT4230 | 32 MB | 32 MB | 512 KB | |
XBTGT2930 | 64 MB | 16 MB | 512 KB | |
XBTGT2430 | 64 MB | 32 MB | 512 KB | |
XBTGT2330 | 32 MB | 16 MB | 512 KB | |
XBTGT2220 | 32 MB | 16 MB | 512 KB | |
XBTGT2130 | 32 MB | 16 MB | 512 KB | |
XBTGT2120 | 32 MB | 16 MB | 512 KB | |
XBTGT2110 | 32 MB | 16 MB | 128 KB | |
XBTGT1335 | 32 MB | 32 MB | 128 KB | |
XBTGT1135 | 32 MB | 32 MB | 128 KB | |
XBTGT1105 | 32 MB | 32 MB | 128 KB | |
Magelis XBTGC Series | XBTGC1100T | 32 MB | 16 MB | 512 KB |
XBTGC1100U | 32 MB | 16 MB | 512 KB | |
XBTGC2120T | 32 MB | 16 MB | 512 KB | |
XBTGC2120U | 32 MB | 16 MB | 512 KB | |
XBTGC2230T | 32 MB | 16 MB | 512 KB | |
XBTGC2230U | 32 MB | 16 MB | 512 KB | |
XBTGC2330T | 32 MB | 16 MB | 512 KB | |
XBTGC2330U | 32 MB | 16 MB | 512 KB | |
Magelis XBTGH Series | XBTGH2460 | 64 MB | 32 MB | 512 KB |
Magelis XBTGK Series | XBTGK2120 | 32 MB | 16 MB | 512 KB |
XBTGK2330 | 32 MB | 16 MB | 512 KB | |
XBTGK5330 | 32 MB | 32 MB | 512 KB | |
Magelis HMIGK Series | HMIGK2310 | 128 MB | 96 MB | 512 KB |
HMIGK5310 | 128 MB | 96 MB | 512 KB |
*1 The XBTGT5430 model comes in two versions that differ in their DRAM size (32 MB or 64 MB). To determine the version of the XBTGT5430, look for the following serial numbers on the manufacturer's label on your target machine:
- 32 MB: PV: 01, RL: 00, SV: 1.0
- 64 MB: PV: 01, RL: 01, SV: 1.1
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: