{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What potentiometer does Schneider-Electric recommend for Altivar drives?

Issue :
Speed potentiometer that Schneider-Electric recommend for Altivar drives.

Product Line :
Altivar Drives

Environment :
Open style drive

Cause :
Speed pot selection

Resolution :
Any pot within the specification of the drive should work.  For all of our Drive products a potentiometer between 2.5kOhm and 10kOhm will do.  The part number ATVPOT25K - 22mm once used for our drives but it may no longer be available.
Below are some of the readily available part numbers typically used with Schneider drives :

For 22mm
Metal - XB4BD912R10K
Plastic - XB5AD912R10K

For 30mm
Metal - 9001K2108
Plastic - 9001SK2108

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: