{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What actions should be taken if a Unity Momentum PLC exhibits an EC10 or EC00 crash error?

Issue
This resolution explains what actions to take if a Unity Momentum PLC exhibits an EC10 or EC00 crash error.


Product Line
171CBU78090
171CBU98090
171CBU98091


Resolution
The Unity Momentum PLC crash error ‘EC10’ or 'EC00' in %SW124 is resolved by upgrading to firmware versions 2.00 or higher and then reload the program.

It is highly recommended to upgrade to the latest released firmware version.

Schneider Electric Nigeria